Links User Guide Reference Apache Tomcat Development | Apache Tomcat 6.0JNDI Datasource HOW-TOIntroduction |
JNDI Datasource configuration is covered extensively in the
JNDI-Resources-HOWTO. However, feedback from tomcat-user has
shown that specifics for individual configurations can be rather tricky.
Here then are some example configurations that have been posted to
tomcat-user for popular databases and some general tips for db usage.
You should be aware that since these notes are derived from configuration
and/or feedback posted to tomcat-user YMMV :-). Please let us
know if you have any other tested configurations that you feel may be of use
to the wider audience, or if you feel we can improve this section in anyway.
Please note that JNDI resource configuration changed somewhat between
Tomcat 5.0.x and Tomcat 5.5.x. You will most likely need to modify older
JNDI resource configurations to match the syntax in the example below in order
to make them work in Tomcat 6.x.x.
Also, please note that JNDI DataSource configuration in general, and this
tutorial in particular, assumes that you have read and understood the
Context and
Host configuration references, including
the section about Automatic Application Deployment in the latter reference.
|
Database Connection Pool (DBCP) Configurations |
DBCP provides support for JDBC 2.0. On systems using a 1.4 JVM DBCP
will support JDBC 3.0. Please let us know if you have used DBCP and its
JDBC 3.0 features with a 1.4 JVM.
See the
DBCP documentation for a complete list of configuration parameters.
Installation |
DBCP uses the Commons Database Connection Pool. It relies on
number of Commons components:
- Commons DBCP
- Commons Pool
These libraries are located in a single JAR at
$CATALINA_HOME/lib/tomcat-dbcp.jar . However,
only the classes needed for connection pooling have been included, and the
packages have been renamed to avoid interfering with applications.
|
Preventing dB connection pool leaks |
A database connection pool creates and manages a pool of connections
to a database. Recycling and reusing already existing connections
to a dB is more efficient than opening a new connection.
There is one problem with connection pooling. A web application has
to explicitly close ResultSet's, Statement's, and Connection's.
Failure of a web application to close these resources can result in
them never being available again for reuse, a db connection pool "leak".
This can eventually result in your web application db connections failing
if there are no more available connections.
There is a solution to this problem. Commons DBCP can be
configured to track and recover these abandoned dB connections. Not
only can it recover them, but also generate a stack trace for the code
which opened these resources and never closed them.
To configure a DBCP DataSource so that abandoned dB connections are
removed and recycled add the following attribute to the
Resource configuration for your DBCP DataSource:
When available db connections run low DBCP will recover and recycle
any abandoned dB connections it finds. The default is false .
Use the removeAbandonedTimeout attribute to set the number
of seconds a dB connection has been idle before it is considered abandoned.
 |  |  |  | removeAbandonedTimeout="60"
|  |  |  |  |
The default timeout for removing abandoned connections is 300 seconds.
The logAbandoned attribute can be set to true
if you want DBCP to log a stack trace of the code which abandoned the
dB connection resources.
The default is false .
|
MySQL DBCP Example |
0. Introduction
Versions of MySQL and JDBC drivers that have been reported to work:
- MySQL 3.23.47, MySQL 3.23.47 using InnoDB,, MySQL 3.23.58, MySQL 4.0.1alpha
- Connector/J 3.0.11-stable (the official JDBC Driver)
- mm.mysql 2.0.14 (an old 3rd party JDBC Driver)
Before you proceed, don't forget to copy the JDBC Driver's jar into $CATALINA_HOME/lib .
1. MySQL configuration
Ensure that you follow these instructions as variations can cause problems.
Create a new test user, a new database and a single test table.
Your MySQL user must have a password assigned. The driver
will fail if you try to connect with an empty password.
 |  |  |  | mysql> GRANT ALL PRIVILEGES ON *.* TO javauser@localhost
-> IDENTIFIED BY 'javadude' WITH GRANT OPTION;
mysql> create database javatest;
mysql> use javatest;
mysql> create table testdata (
-> id int not null auto_increment primary key,
-> foo varchar(25),
-> bar int);
|  |  |  |  |
Note: the above user should be removed once testing is
complete!
Next insert some test data into the testdata table.
 |  |  |  | mysql> insert into testdata values(null, 'hello', 12345);
Query OK, 1 row affected (0.00 sec)
mysql> select * from testdata;
+----+-------+-------+
| ID | FOO | BAR |
+----+-------+-------+
| 1 | hello | 12345 |
+----+-------+-------+
1 row in set (0.00 sec)
mysql>
|  |  |  |  |
2. Context configuration
Configure the JNDI DataSource in Tomcat by adding a declaration for your
resource to your Context.
For example:
 |  |  |  | <Context path="/DBTest" docBase="DBTest"
debug="5" reloadable="true" crossContext="true">
<!-- maxActive: Maximum number of dB connections in pool. Make sure you
configure your mysqld max_connections large enough to handle
all of your db connections. Set to -1 for no limit.
-->
<!-- maxIdle: Maximum number of idle dB connections to retain in pool.
Set to -1 for no limit. See also the DBCP documentation on this
and the minEvictableIdleTimeMillis configuration parameter.
-->
<!-- maxWait: Maximum time to wait for a dB connection to become available
in ms, in this example 10 seconds. An Exception is thrown if
this timeout is exceeded. Set to -1 to wait indefinitely.
-->
<!-- username and password: MySQL dB username and password for dB connections -->
<!-- driverClassName: Class name for the old mm.mysql JDBC driver is
org.gjt.mm.mysql.Driver - we recommend using Connector/J though.
Class name for the official MySQL Connector/J driver is com.mysql.jdbc.Driver.
-->
<!-- url: The JDBC connection url for connecting to your MySQL dB.
-->
<Resource name="jdbc/TestDB" auth="Container" type="javax.sql.DataSource"
maxActive="100" maxIdle="30" maxWait="10000"
username="javauser" password="javadude" driverClassName="com.mysql.jdbc.Driver"
url="jdbc:mysql://localhost:3306/javatest"/>
</Context>
|  |  |  |  |
3. web.xml configuration
Now create a WEB-INF/web.xml for this test application.
 |  |  |  | <web-app xmlns="http://java.sun.com/xml/ns/j2ee"
xmlns:xsi="http://www.w3.org/2001/XMLSchema-instance"
xsi:schemaLocation="http://java.sun.com/xml/ns/j2ee
http://java.sun.com/xml/ns/j2ee/web-app_2_4.xsd"
version="2.4">
<description>MySQL Test App</description>
<resource-ref>
<description>DB Connection</description>
<res-ref-name>jdbc/TestDB</res-ref-name>
<res-type>javax.sql.DataSource</res-type>
<res-auth>Container</res-auth>
</resource-ref>
</web-app>
|  |  |  |  |
4. Test code
Now create a simple test.jsp page for use later.
 |  |  |  | <%@ taglib uri="http://java.sun.com/jsp/jstl/sql" prefix="sql" %>
<%@ taglib uri="http://java.sun.com/jsp/jstl/core" prefix="c" %>
<sql:query var="rs" dataSource="jdbc/TestDB">
select id, foo, bar from testdata
</sql:query>
<html>
<head>
<title>DB Test</title>
</head>
<body>
<h2>Results</h2>
<c:forEach var="row" items="${rs.rows}">
Foo ${row.foo}<br/>
Bar ${row.bar}<br/>
</c:forEach>
</body>
</html>
|  |  |  |  |
That JSP page makes use of JSTL's SQL and Core taglibs. You can get it from Sun's Java Web Services Developer Pack or Jakarta Taglib Standard 1.1 project - just make sure you get a 1.1.x release. Once you have JSTL, copy jstl.jar and standard.jar to your web app's WEB-INF/lib directory.
Finally deploy your web app into $CATALINA_BASE/webapps either
as a warfile called DBTest.war or into a sub-directory called
DBTest
Once deployed, point a browser at
http://localhost:8080/DBTest/test.jsp to view the fruits of
your hard work.
|
|
Non-DBCP Solutions |
These solutions either utilise a single connection to the database (not recommended for anything other
than testing!) or some other pooling technology.
|
Oracle 8i with OCI client |
Introduction |
Whilst not strictly addressing the creation of a JNDI DataSource using the OCI client, these notes can be combined with the
Oracle and DBCP solution above.
In order to use OCI driver, you should have an Oracle client installed. You should have installed
Oracle8i(8.1.7) client from cd, and download the suitable JDBC/OCI
driver(Oracle8i 8.1.7.1 JDBC/OCI Driver) from otn.oracle.com.
After renaming classes12.zip file to classes12.jar
for Tomcat, copy it into $CATALINA_HOME/lib .
You may also have to remove the javax.sql.* classes
from this file depending upon the version of Tomcat and JDK you are using.
|
Putting it all together |
Ensure that you have the ocijdbc8.dll or .so in your $PATH or LD_LIBRARY_PATH
(possibly in $ORAHOME\bin ) and also confirm that the native library can be loaded by a simple test program
using System.loadLibrary("ocijdbc8");
You should next create a simple test servlet or jsp that has these
critical lines:
 |  |  |  | DriverManager.registerDriver(new
oracle.jdbc.driver.OracleDriver());
conn =
DriverManager.getConnection("jdbc:oracle:oci8:@database","username","password");
|  |  |  |  |
where database is of the form host:port:SID Now if you try to access the URL of your
test servlet/jsp and what you get is a
ServletException with a root cause of java.lang.UnsatisfiedLinkError:get_env_handle .
First, the UnsatisfiedLinkError indicates that you have
- a mismatch between your JDBC classes file and
your Oracle client version. The giveaway here is the message stating that a needed library file cannot be
found. For example, you may be using a classes12.zip file from Oracle Version 8.1.6 with a Version 8.1.5
Oracle client. The classeXXXs.zip file and Oracle client software versions must match.
- A
$PATH , LD_LIBRARY_PATH problem.
- It has been reported that ignoring the driver you have downloded from otn and using
the classes12.zip file from the directory
$ORAHOME\jdbc\lib will also work.
Next you may experience the error ORA-06401 NETCMN: invalid driver designator
The Oracle documentation says : "Cause: The login (connect) string contains an invalid
driver designator. Action: Correct the string and re-submit."
Change the database connect string (of the form host:port:SID ) with this one:
(description=(address=(host=myhost)(protocol=tcp)(port=1521))(connect_data=(sid=orcl)))
Ed. Hmm, I don't think this is really needed if you sort out your TNSNames - but I'm not an Oracle DBA :-)
|
|
Common Problems |
Here are some common problems encountered with a web application which
uses a database and tips for how to solve them.
Intermittent dB Connection Failures |
Tomcat runs within a JVM. The JVM periodically performs garbage collection
(GC) to remove java objects which are no longer being used. When the JVM
performs GC execution of code within Tomcat freezes. If the maximum time
configured for establishment of a dB connection is less than the amount
of time garbage collection took you can get a db conneciton failure.
To collect data on how long garbage collection is taking add the
-verbose:gc argument to your CATALINA_OPTS
environment variable when starting Tomcat. When verbose gc is enabled
your $CATALINA_BASE/logs/catalina.out log file will include
data for every garbage collection including how long it took.
When your JVM is tuned correctly 99% of the time a GC will take less
than one second. The remainder will only take a few seconds. Rarely,
if ever should a GC take more than 10 seconds.
Make sure that the db connection timeout is set to 10-15 seconds.
For the DBCP you set this using the parameter maxWait .
|
Random Connection Closed Exceptions |
These can occur when one request gets a db connection from the connection
pool and closes it twice. When using a connection pool, closing the
connection just returns it to the pool for reuse by another request,
it doesn't close the connection. And Tomcat uses multiple threads to
handle concurrent requests. Here is an example of the sequence
of events which could cause this error in Tomcat:
Request 1 running in Thread 1 gets a db connection.
Request 1 closes the db connection.
The JVM switches the running thread to Thread 2
Request 2 running in Thread 2 gets a db connection
(the same db connection just closed by Request 1).
The JVM switches the running thread back to Thread 1
Request 1 closes the db connection a second time in a finally block.
The JVM switches the running thread back to Thread 2
Request 2 Thread 2 tries to use the db connection but fails
because Request 1 closed it.
Here is an example of properly written code to use a db connection
obtained from a connection pool:
Connection conn = null;
Statement stmt = null; // Or PreparedStatement if needed
ResultSet rs = null;
try {
conn = ... get connection from connection pool ...
stmt = conn.createStatement("select ...");
rs = stmt.executeQuery();
... iterate through the result set ...
rs.close();
rs = null;
stmt.close();
stmt = null;
conn.close(); // Return to connection pool
conn = null; // Make sure we don't close it twice
} catch (SQLException e) {
... deal with errors ...
} finally {
// Always make sure result sets and statements are closed,
// and the connection is returned to the pool
if (rs != null) {
try { rs.close(); } catch (SQLException e) { ; }
rs = null;
}
if (stmt != null) {
try { stmt.close(); } catch (SQLException e) { ; }
stmt = null;
}
if (conn != null) {
try { conn.close(); } catch (SQLException e) { ; }
conn = null;
}
}
|
Context versus GlobalNamingResources |
Please note that although the above instructions place the JNDI declarations in a Context
element, it is possible and sometimes desirable to place these declarations in the
GlobalNamingResources section of the server
configuration file. A resource placed in the GlobalNamingResources section will be shared
among the Contexts of the server.
|
JNDI Resource Naming and Realm Interaction |
In order to get Realms to work, the realm must refer to the datasource as
defined in the <GlobalNamingResources> or <Context> section, not a datasource as renamed
using <ResourceLink>.
|
|
|